AXIS#.MT​.DISALLOWINTERRUPT

Description

This parameter sets the motion task control word specifying whether or not to be able to interrupt the current motion task.

It takes the following values:

Value Description
0 Allow Interrupt
1 Disallow Interrupt

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.DISALLOWINTERRUPT Will configure Motion Task 0 to disallow being interrupted.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write Array
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Start Version  

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.DISALLOWINTERRUPT 0

50deh

01h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 1

50deh

02h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 2

50deh

03h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 3

50deh

04h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 4

50deh

05h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 5

50deh

06h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 6

50deh

07h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 7

50deh

08h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 8

50deh

09h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 9

50deh

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 10

50deh

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 11

50deh

0ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 12

50deh

0dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 13

50deh

0eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 14

50deh

0fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 15

50deh

10h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 16

50deh

11h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 17

50deh

12h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 18

50deh

13h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 19

50deh

14h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 20

50deh

15h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 21

50deh

16h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 22

50deh

17h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 23

50deh

18h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 24

50deh

19h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 25

50deh

1ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 26

50deh

1bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 27

50deh

1ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 28

50deh

1dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 29

50deh

1eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 30

50deh

1fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWINTERRUPT 31

50deh

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6314

1

6314 (0x18aa)

AXIS1.MT.DISALLOWINTERRUPT

Unsigned8[32]

Read/Write

Yes

71850

2

6314 (0x18aa)

AXIS2.MT.DISALLOWINTERRUPT

Unsigned8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.DISALLOWINTERRUPT

6314

Unsigned8[32]

Read/Write

-